Cooling Towers

Where can I find the Full Load Amps (FLA) of a cooling tower’s electrical components?

A unit’s motor full load amps (or FLA) can be found in the technical data sheet for each specific cooling tower.  It is also located in EVAPCO’s custom selection software, Spectrum, in the returned results table. To determine the FLA for other electrical accessories, please contact...

How do I clean my air inlet louvers?

Cooling towers can often experience mineral/scale buildup on the exterior surfaces of their air inlet louvers. Improper water treatment, insufficient bleed rates, and/or excessive cycling of the fan motors are the most typical causes. Since the louver material is constructed of lightweight PVC, it cannot withstand the rigors of heavy...

What are the benefits of a belt drive system when compared to a gear box drive system?

A belt drive system brings many advantages including lower upfront costs, simplified maintenance, lower replacement costs, and shorter lead time.

Regarding maintenance, belt drive systems are much easier to service than gear box drive systems as they require no special tools, equipment, or skills.  EVAPCO cooling towers...

What is the minimum recommended fan speed for an open cooling tower?

EVAPCO recommends a minimum fan speed of 25% for each available open cooling tower. Operating below 25% of motor speed achieves very little return in fan energy savings and capacity control. This recommend also applies to closed circuit coolers and evaporative condensers. If you have additional questions about the operation...

Why would I use equalizer connections instead of a flume box?

Water equalization is required anytime there are two or more separate basins that are combined on the same condenser water loop. There are two main types of equalization: flume box or external equalizer pipe. Only one of these options is required.  

 The default equalization...

Fluid Coolers

What is a dry bulb switchover temperature?

A dry bulb switchover temperature refers to the temperature at which a closed circuit cooler can run fully dry (with just the fans running, without the spray pumps on) and reject 100% of the design heat load. This is an important term in the engineering community as a higher dry...

Can I operate my closed circuit cooler recirculating pump on a VFD?

No, the recirculating pumps supplied on EVAPCO closed circuit coolers are ON/OFF and require full flow to maintain system efficiency and prevent premature scaling of the coil. They are not designed to operate on a variable frequency drive (VFD).

Every fluid cooler pump is sized for a set flow rate...

When should I use glycol in my closed loop system instead of water?

Glycol has antifreeze properties that protect coils in a closed circuit cooler from potential freezing during winter operation in northern climates.  Glycol solutions are rarely used for closed loop systems in warmer climates, such as Florida or Arizona, unless they are being used as corrosion inhibitors.

In general, about half...

Where can I find the coil volume of my closed circuit cooler?

You can find the coil volume of your closed circuit cooler in 3 places. Each model’s product brochure contains this important information. Visit our comprehensive Document Library to locate up-to-date materials related to your specific fluid cooler. You may also find the coil volume in the project submittal, or within EVAPCO’s selection...

Why do I need to maintain a minimum flow in my closed circuit cooler? What is the minimum flow I must maintain?

A minimum flow needs to be maintained in all closed circuit coolers to prevent potential freezing/bursting of the coil(s) during cold weather operation. Also, when the flow falls below a certain threshold it becomes laminar, which will significantly reduce performance during normal operation. The recommended minimum flow for each EVAPCO...

Water Systems

How does the quality of my site’s makeup water impact water efficiency or influence materials of construction decisions?

Water originates from various sources and can vary significantly in quality. Makeup water contains invisible dissolved minerals and insoluble matter that can impact cooling efficiency and equipment service life. These substances include dirt, minerals, gases, and microbiological organisms that, if not properly treated, can accumulate and cause reductions in heat...

How does the need for immediate heat load affect galvanized steel coils?

For decades, the evaporative cooling industry has relied on galvanized steel as a preferred material of construction due to its cost effectiveness and thermal performance.  

Galvanized zinc provides corrosion protection for the underlying carbon steel. This zinc layer is both a protective layer and acts as a sacrificial anode...

What are the environmental, health & safety benefits of non-chemical or solid chemical water treatment programs for evaporative cooled systems?

EVAPCO® Water Systems offers advanced water treatment programs tailored to the specific needs of evaporative cooling systems, considering factors such as makeup water quality, unit type, and location. Two key solutions, Pulse~Pure® and Smart Shield®, are available for open cooling towers, closed circuit coolers, and evaporative condensers. These systems...

What risks, if any, are associated with using municipal reclaim, rainwater or softened water as makeup for my evaporative cooled system?

Questions regarding alternative makeup water sources for evaporative cooling have become more prevalent due to water scarcity and water usage concerns. These alternate sources of makeup water can be evaluated if the system is designed to provide consistent makeup water quality to the evaporatively cooled system. The following should be...

Without increasing my system’s cycles of concentration, how can I reduce blowdown and makeup water demand?

Water is required for energy efficient evaporative cooling commonly used in HVAC, refrigeration, and industrial process cooling systems. Water demand for these cooling systems can be significant. As the global water crisis grows, reducing water usage in these systems becomes more and more important. EVAPCO’s industry’s leading dry and adiabatic...

Parts & Maintenance

Can EVAPCO provide replacement parts for another manufacturer's cooling tower?

Yes.  EVAPCO can provide replacement parts for any piece of cooling equipment you have onsite.  For specific parts and pricing (or custom requests), please contact your local sales representative.

EVAPCO has been offering parts for non-EVAPCO cooling equipment for many years.  We have a dedicated Custom Design Team, as part...

How long (in general) does cooling tower fill last?

Typically, heat transfer media (otherwise known as fill) will need to be replaced once or twice during the life of a cooling tower.The longevity of fill, or heat transfer media, is predominantly a function of water and air quality, as well as proper operation.  If you believe you need replacement...

I need to improve the maintenance access to my cooling tower, condenser, or fluid cooler. Can EVAPCO custom fabricate ladders and service platforms to fit my installation requirements?

Yes, we can! Our representatives will work with you to provide a ladder and/or service platform designed to meet your needs and budget. The Custom Design Team within our Mr. Goodtower® division is able to fabricate solutions, even for non-EVAPCO equipment.

Our goal is to provide safe and secure serviceability for your...

My cooling tower is not functioning as well as it did when it was new. Is this normal? How do I get it running back to normal?

Over time, cooling tower performance can degrade due to a variety of factors. This is completely normal; however, your local EVAPCO sales representatives can help to improve operation. Our team of representatives and Mr. Goodtower® Service Centers are experts in cooling equipment and replacement parts.

If you notice any potential issues...

Troubleshooting

My cooling tower is overflowing because the mechanical float valve is stuck open. What should I do?

The mechanical float valve that EVAPCO uses operates with a makeup water pressure between 20 and 50 psi.  When the makeup water pressure exceeds the 50-psi limit, the makeup valve will not close.  The reason for this is that the buoyant force of...

My tower was just installed and there is rust around the basin. What can I do?

If the unit was just installed, the rust is probably not affecting the integrity, or life expectancy, of the base stainless steel material.  It is most likely foreign material on the surface that can be cleaned. 

So, where is the rust coming from?  The rust spots that show up on the surface of the unit are...