Renewable energy enthusiasts now have reason to celebrate: EVAPCO offers a solar-powered evaporative cooling tower. The SUN cooling tower, available in two sizes — 241 and 383 nominal tons — is paired with PV panels to dramatically reduce energy consumption.
The SUN cooling tower is capable of achieving net-zero operation because its 9 or 12 photovoltaic (PV) solar panels power the unit fully at 50% capacity. Its net-zero capability stems from an annual average of energy usage (most of the year, evaporative cooling towers operate at less than 50% of their capability).
Read the entire article here: ACHR News